Other Parts Discussed in Thread: TPS65133,
Hi,
I am working on a HiFi audio project and considering Ti's TPS65130 or TPS65133 for Operational Amplifier Supplies. according to the datasheet, the TPS65133 seems to be more suitable but output votlage is fixed at +/- 5Vdc only. while the TPS65130 can provide higher output voltage but I am worried about its ripple & noise. so appreciate if you can let me know if the TPS65130 is suitbale for Operational Amplifier Supplies as well. if using an ultra-low-noise LDO to connect to the output of TPS65130, is it helpful to reduce ripple & noise ?
Thanks.
Felix