Hi Team,
Is there any data of input current of EN pin?
I believe the value is "± a few uA" at most but wants to know it just for reference.
Best Regards,
Yaita / Japan disty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yaita-san,
It is around 1-3uA based on the voltage level on the EN pin. If VEN=2V, then it is around 2uA.
Hi Helen-san,
Thank you for your kind support!
1)
I believe input current is around ±(1-3 uA) when VEN=0V?
Is my understanding correct?
2)
Is the following actual measured value? (design value?)
>It is around 1-3uA based on the voltage level on the EN pin. If VEN=2V, then it is around 2uA.
Best Regards,
Yaita
Hi Yaita-San,
Please check my reply below:
1)
I believe input current is around ±(1-3 uA) when VEN=0V?
Is my understanding correct?
--> what do u mean by input current? Iin or Ien flow into the EN pin?
2)
Is the following actual measured value? (design value?)
It is around 1-3uA based on the voltage level on the EN pin. If VEN=2V, then it is around 2uA.
--> This is a design value, there's a resistor internally connects from the EN to GND, which is around 1M ohm.
Hi,
Thank you for your support!
1)
I believe input current is around ±(1-3 uA) when VEN=0V?
Is my understanding correct?
--> what do u mean by input current? Iin or Ien flow into the EN pin?
--> I mean "Ien flow into the EN pin" when VEN=0V.
Best Regards,
Yaita
Hi Yaita,
When VEN=0, the IC is in shutdown mode. the current will flow into the VIN pin and SW pin, which is less than 3uA totally. There's nearly no current flow into the EN pin.