Other Parts Discussed in Thread: CSD86311W1723, CSD85302L, CSD85301Q2
Hi,
We are planning to use n-channel e mosfet between battery and rest of the circuit.
We need the mosfet to turn off when gate voltage is low and turn on when gate voltage is high.
Current rating should be more than 1A with low Rds-on and voltage rating should be more than 4.2V
Also the mosfet should be bidirectional (drain to source as well as source to drain). Basically when mosfet is ON we need it to support charging of battery as well as discharging supply to the circuit depending on voltage level whichever is high.
Can you suggest few n channel e-mosfet and also let me know if this configuration will work?
Thanks in advance.
Regards,
Rahul