This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS561201: TPS561201 Feedback Value

Part Number: TPS561201


Hello,

we want to take a TPS561201 to generate 5.4V from a 12V source. In the datasheet VFB is defined with typ 0.768V. We take 10k as R1 and 60.4k as R2 and we are expecting 5.4V. But we are measuring 0.8V at the VFB and 5.59V at the output. We are not understanding the datasheet, because there is given IVFB=0µA at 0.8V. Is it correct?

What is the right value of the voltage regulator?

Thank you

Regards Michael