This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51206: VLH,min for VDD = 3.3V

Part Number: TPS51206

The data sheet page 5 indicates that the VLH,min for S3, S5 is 1.8V when VDD = 5V.

I am using VDD = 3.3V.

What is VLH,min when VDD = 3.3V?

Thanks, Best, Steve