Other Parts Discussed in Thread: TPS61085, TPS7A30,
Hello.
Two questions about this part:
1- May I set the SS for say 50ms?
2- Can it stand a few watts during this interval?
To put this into context, I am going to use this LDO (and the TPS7A30 too for that matter) to post-regulate the output of a +15.5V/50mA boost supply (ADP5073 buck/boost inverter, -15.5V/50mA in TPS7A30 case). However, the capacitance at the LDO output is about 400uF. The inverter does not start with such a high capacitance (on simulator). I did not simulate the boost inverter yet (TPS61085) but I suspect something similar will happen. I am thinking of controlling the LDOs with the power-good outputs of the converters and set them to a reasonably slow (around 50ms) time. So, during a short time the LDO will sink a relatively high power, starting with a few watts and reducing as the capacitor voltages reaches the operating voltages (+/- 14.0V). Can the LDOs stand this power for this time?
Is the scheme described above OK? Would you suggest another approach?