We just completed a design with the UCD9240 (80-pin version) and we are in the testing stages. The design is as close as being 'by the book' as it gets with the caveats that the documentation is not consistent with respect to the connection of some pins (e.g., leave floating, or connect a resistor/capacitor to them). We have used development board schematics (from TI and XILINX) to resolve those inconsistencies. To minimize any risk, we went as far as using TI recommended parts for nearly all design decisions.
The modules are running off a regulated 5V power bus (which comes from yet another TI module).
The same exact issues were seen in three separate test boards (all three prototypes tested).
Among the many issues we have had:
- All measurements (inputs and outputs) are consistently 10% below the programmed value. We have had to 'lie' to the fusion interface to get them to the proper set points.
- The 3.3V regulator has a 3.1V output. We had to reduce the bias resistor to get it to 3.3V, and this node is overly sensitive to the resistor value. And yes, we followed all the equations in the design guides, the value we had to use is below the minimum given by the equations and nearly an order of magnitude below the maximum acceptable value.
- The BPCAP node, measured with a high-impedance voltmeter, is at 1.65V (instead of the nominal 1.8V). Which could explain the rest of the problems.
These parts were supposed to be factory-calibrated to better than 5%, and I don't see a calibration constant that would remove such gain/scale error. What is going on here?