I have completed one design with the UCD9240 (80 pin version) but I still have some design issues due to datasheet inconsistencies. Namely:
What to do with the ADCREF pin? Depending on what documentation I follow this pin:
- should be left floating when unused.
- should be bipassed with a .1uF capacitor to gnd.
- can be used for an external 1.6V reference.
What is this pin purpose, what should I do with it?
What design criteria should we use for V33FB? Depending on the document this pin should have
- 10mA _typical_ design current (no minimum)
- 10mA _maximum_ design current (no minimum), with 5mA recommended as a guideline.
After following design guidelines, using 4mA as a target resulting in a resistance range from 300Ω to 1KΩ , during testing I had to further reduce it to 220Ω to get a reasonable voltage out (within 5%), with a very high dependency in this resistor value. Is this output even regulated in any real sense? (The documentations is not clear on this point either.)