Other Parts Discussed in Thread: BQ78350
Hi,
I would like to upgrade my BSM with handle external potential meter as input and do data massage (figure 2,) rather than the external potential on Controller / loading side (figure 3.), however with both control signal connected together mean both GROUND has to be connected together (figure 1.) imagine when PACK- and PACK+ connect to LOADING spike appear because LOADING ground is equal BSM ground, my existing design is both CHG and DSG is connected by MCU so that without MCU command the path was disconnected to prevent spike or inrush current, also now measuring discharge current look strange.
Can anyone help to review my design ? do I need to isolate both GROUNDs ? any TI ic solution help ?
Tiger