Part Number: BQ24133
Hi Community,
We are using the above device to charge two cell LIPO batteries. Everything works good.
I want to know the behavior of the IC when there is no external charging voltage present and the
battery is being discharged to load via via the BATFET controlled via the /BATDRV signal.
What happens when the LIPO is fully discharged to say 6.5V (8.2V fully charged) does the BATDRV
turn off and isolate the battery from the load so that the LIPO is protected?
This is very important to us as we don't want the battery to continue to discharge into the load
when it is fully discharged as it can damage the LIPO. I was reading about UVLO but this voltage
seems to be for the single cell configuration.
Your comments regarding the above is valued.
Regards
Manjula