This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256303: help provide coefficients for LLC inductor

Part Number: UCC256303

As for or UCC256303, the The system parameters are below:

Vout  :55.5V  , Iout:10A   Pout:555W

Vin-nom:150V,  Vin-max:180V,   Vin-min:120V,  

LLC frequency 100kHz

Could you help provide the coefficients for the LLC inductor design?