Other Parts Discussed in Thread: UCC25630-1EVM-291,
Dear support member,
My customer used UCC 256304.
Although it was evaluated with 2ch output from UCC25630-1EVM-291,
Duty cycle was not 50%.
Q1
What is the cause?
Q2
Where should I check?
Specification condition
Vin: 140 V
Vout 1: 12V
Iout 1: 3A
Vout 2: 60V
Iout 3: 1A
Best regard.
Bob Lee.