This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24780S: Charger doesn't disconnect battery from system when charging

Part Number: BQ24780S


Hi, we are using the BQ24780s in a design with a 4 cells battery. Most of our boards works fine, but one of them doesn't .When we connect the AC, the charger connects it to the system, but does not disconnect the battery from the system. We use a 19 V supply with the 16.8V battery. If the battery is around 14 V, BATSRC is at 14 V and BATDRV is at 20 V, everything is normal. When we connect the AC, the BATSRC goes up to 18.4 V and BATDRV to 24.4 V. On a working board, both BATSRC and BATDRV are equal to the battery voltage.

Any idea on what can cause this kind of behaviour?

Regards,
Leonard