This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200: What is the total tolerance on Vout w.r.t Refin

Part Number: TPS51200


Hi Team,

What is the total tolerance on Vout w.r.t Refin?

REFIN  to Refout tolerance is 15mV & Vout to Refout tolerance is listed as 25mV,

So, is the total tolerance the RSS (Root Sum of Squares) sum of these two errors or direct addition of them? 

Reards,

Praveen