This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53681: Setting Vout to 5V and 3.3V

Part Number: TPS53681


Hello,
I am having a similar situation to the one described in e2e.ti.com/.../707586
I would like to generate 3.3V from a 12V nominal input rail (but it can range from 9 to 14V) using channel B of this Buck controller.
Reading the datasheet I cannot find any reason why it should not be possible to generate such output voltage level using a divider network on the feedback pin BVSP.
Is it possible to know the additional modifications, other than the voltage divider network, needed to generate higher Vout with this component?
Thanks

Best regards,

Simone