Hi,
I am using TPS561201 and input is 15V and output is 3.3V.
Now I want to add feature (low cost) so that on power down microcontroller get some time to save parameter and send information. Typical load in this duration is about 150mA and time is 100msec
Now can I use 1000uf ~2000uf capacitor at the output of TPS561201 which provided charging when the input 15V disappear.
Regards,