Part Number: TPS43060
Other Parts Discussed in Thread: TPS43061, LM5069
We have a scenario where the TPS43060 is on a fully biased, operating properly.
Vin = 28V, Vout = 51V, up to 5A of output current. The TPS43061 is powered separately by 12V bias rail, i.e. pin 7 = 12V.
Vin is momentarily glitched due to an erroneous cut-out of an up-stream hot-swap controller (LM5069), and afterward we find that the TPS43060 is dead.
I suspect that the glitch is lasting only a few milli seconds, and during the glitch the EN of TPS43060 is held high constantly.
This glitch is related to the bouncing of a switch, and may not be a single event, and not consistent.
Under these conditions, the output capacitance (~50 uF) is probably not fully discharging, and when Vin comes back, the regulator is now facing a pre-biased but browned-out output voltage.
I imagine that the error amp is likely railed high trying to compensate, the SS is not reset, and when Vin comes back it takes some time to close the loop again.
Can you provide any insight into how the TPS43060 will behave under these circumstances?
I would think that cycle-by-cycle current limiting would protect the device?
We will update the design to clean up any bouncing, but we would like to better understand what happened that blew up the device.
Also, upon reviewing the design, I see that we are missing the required Rcharge = 2 Ohm resistor in series with the bootstrap diode.
We will fix this as well, but I mention it in case it is important to this issue.
Thanks, Best, Steve