Hi,
I noticed that at the end of the datasheet in section 8.2.1 Design Requirement (page 49), the max discharge current is set to 10A.
I was wondering whether it is possible to use this chip for higher power applications such as a 9s10p battery with peak discharge of ~100A? if not, does TI offer any other solution for this case?
thank you