This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: First charge cycle only goes to 98%

Part Number: BQ40Z50

I have made a BMS based on the BQ40Z50. Did the learning cycle, Made a golden file.

First time the packs charge, most stop around 98% and never get to 99% or 100% (I have bit set to require EOC success to go to 100%).

Is this because the FCC it learned is higher than the average pack? How can I fix that?