This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78PL114 pack capacity error

Other Parts Discussed in Thread: BQ78PL114

We have a problem with our pack capacity indication. During discharge it goes down linearly from 100% to about 89%. Then jumps down to about 75% and continous again in a linear fashion. However, when it gets to 0%, then is still a considerable amount of charge left. I am referring to the realtive state of charge.

We have calibrated the pack and also done the discharge, charge with pulsing and discharge process prescribed in the application notes, but this does not fix the problem of the jump.

Please advise.

 

  • Hello.

     

    Do you have a problem of oszillating Charge- and Discharge-MOSFETs at the same time? 

     

    I have these problems with the bq20z95 at the same time.  I think, it something goes wrong with the calibration of the pack.

    I am not familiar with the bq78pl114, right now.

    Greetz,

     

    Arne