Other Parts Discussed in Thread: BQ40Z50-R2, BQ40Z50, BQ25713
Hi All,
I'm designing a UPS system that will have an initial battery pack (4 serial Lithium 5.4Ah Cells). This will be the base UPS module.
I then want to add additional capacity to the UPS by adding more battery packs. ie additional board with another group of four series cells and a battery monitor.
The basic main UPS module BOM that I'm looking at will consists of the following:
1 * LTC4357 (Reverse polarity protection)
1 * LT4363 (Surge Suppressors High Voltage Surge Stopper with Current Limit. Auto-Retry after Fault)
1 * BQ24773 (Proposed 5A Battery Charger)
1 * BQ40z50-R2 (Li-Ion Battery Pack Manager)
I expect that the additional battery pack modules will have:
1 * BQ40z50-R2 (Li-Ion Battery Pack Manager)
I will have a micro that will be interfacing to the BQ24773 and BQ40z50-R2. Its power supply will need to come from either a) charger input AND/OR b) a charged battery pack input. Basically ORed together via diodes or such. It will control the charger and talk to the multiple BQ40z50's.
Basically, I will use the micro to switch the charger between various battery packs to either charge the pack from a low state or to perform top-up's.
Question is, how do I connect the additional battery packs to the BQ24773? (I need make before break. So no back feeding of flat battery pack.)
At what point would you suggest placing a switching Mosfet?
Is the BQ24773 the best IC to use in this situation?
Thanks,
Neil