Dear all.
The TPS659039-Q1 is not working and is being checked.
The problem is that RC 32 kHz does not turn out in the datasheet Figure 6-20 and therefore not all DCDC & LDO outputs.
Below are the connections.
| Pin | connection |
| VCC1 | 3.3V |
| VCC_SENSE | 3.3V |
| VCC_SENSE2 | 3.3V |
| PWRON | Pull-up(120k)à3.3V |
| RPWRON | Floating |
| POWERDOWN | Floating |
| BOOT0 | Pull-down |
| BOOT1 | Pull-down |
| RESET_IN | High(3.3V) |
| ENABLE1 | Floating |
| GPIO0 | Pull-down |
| GPIO1 | Floating |
| GPIO2 | Floating |
| GPIO3 | Pull-down |
| GPIO4 | Floating |
| GPIO5 | Pull-down |
| GPIO6 | Floating |
| GPIO7 | Pull-up(10k)àLDOVRTC |
| VPROG | GND |
| VBUS | Pull-down(10k) |
| PWRGOOD | Floating |
| NSLEEP | Floating |
| NRESWARM | Floating |
| VBG | Cap 100nF |
Please advise me on this matter.