This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/BQ27510-G3: GDK ,BQstudio 1.3.76

Part Number: BQ27510-G3

Tool/software: Code Composer Studio

I am using GDK and BQ studio 1.3.76 to get 'golden image' for BQ27510-G3. The 'update status' has changed to '02' and 'Qmax' and 'Ra table' also have updated. Before I export 'golden imgae',  I check the 'dataflash' and change 'discharge current threshold' from 400mA to 2000 mA, NEXT press 'WRITE to ALL '. There is a pump that this data isn't stored. In order to make sure if this data is stored , I close 'dataflash' and reopen it. But I notice that 'update status ' CHANGES to '01'. The golden image doesn't store.

  • Hi
    Why will you want to set the discharge current threshold to such a high value. That doesn't seem correct to me as the gauge may never enter discharge mode. The gauge needs to enter discharge mode for IT algorithm to work properly.

    thanks
    Onyx