This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61170: Compensation constant in case of SEPIC topology

Part Number: TPS61170

Hi all

Would you mind if we ask TPS61170?
Our customer considers follow configuration;
20180809_TPS61170.pdf

And then, we have some guestions about compensation constant in case of SEPIC topology

<Question1>
The datasheet P19 shows, "For many of the applications, the recommended value of 10k and 680pF makes an ideal compromise between transient response and loop stability.".
So, in case of SEPIC topology, does the recommended value of 10k and 680pF make an ideal compromise between transient response and loop stability also?

<Question2>
In relation <Question1>, the datasheet Figure19 shows that compensation constant is 220nF only.
In case of SEPIC topology, should we use 220nF instead of 680pF and 10k?

<Question3>
If you have some recommended value, could you share us?
Or, should we calculate using formula (7) to (10)?

Kind regards,

Hirotaka Matsumoto