hello, Good afternoon.
I am designing an Rf phase shifter at high power around 1KW peak.
The design is carried out using a pin diode which requires -100V for reverse bias.
I got the circuit for 100V as below and modified one is also available as below
I have modified the same for -100V. attached
please suggest for the change if required.
Thank youwebench_esim_5769354_4_2_373495492.pdfupdated_28_100V.pdf