Hi, I'm looking for the bqEVSW that supports the custom chip bq30z55R3 v0.36, I'm using the EV2300
please help..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I'm looking for the bqEVSW that supports the custom chip bq30z55R3 v0.36, I'm using the EV2300
please help..
hi Mohammed,
As you mentioned, bq30z55-R3 is a custom IC so we cannot support your request. Unless you can prove you're working for the OEM or pack maker to whom we're selling this IC.
if you're looking for a catalog multicell gauge, please look at bq40z50-R2.
Regards,
David
First, you should have valid 128-bit sha-1 unseal key which was used at production stage by pack maker to SEAL the gauge.
If you are sure you have it, then unseal process is pretty simple, just use "SEAL AUTH" page of bqEVSW, where you should enter the key in appropriate 'unseal key' field, and to press the 'unseal' button. It will launch unseal sequence, first reading the random challenge from the gauge then sending sha1-hmac response back to gauge. if it's correct, gauge would be unsealed, and you could observe this by appropriate SEC0,SEC1 flags in OPSTATUS register at SBS page.