This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54428: CBST max allowed value

Expert 3040 points

Part Number: TPS54428

Hello, 

Due to MLCC shortage, customer want to use even higher value of C7, if allowed, C7=10uF. 

Basically, huge capacitance takes more time of charging voltage for high-side switch, does this impact on minimum on time, which may be longer than max of specified in d/s?

Please let me know if my understanding is correct or not.

Regards, ny

  • Hi,
    It only affect the behavior at power up. When startup, the 10uF cap took longer time to charge to a proper high value. The cap voltage is used to turn on the HS MOSFET, if the voltage is not high enough, HS MOSFET can't be turned on.
    If the IC power up successfully, Then the IC works normally after that. The minimum on time is not affected.
    10uF is quite a big value, we haven't qualified that, and need to experiment to verify. Please check at Vinmin, Voutmax, Ioutmin on your board, to check the power up process.
  • Hi Zhang, thank you very much