This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28711: UCC28711

Part Number: UCC28711
Other Parts Discussed in Thread: TIDA-00173

I try to use UCC28711 to design a auxiliary Power for 380V AC Motor Control. The input voltage is 540V DC, and the MAX voltage maybe high to 1200V DC.The out put of the auxiliary power with two output,one is 15VDC 300mA,and the other is 12VDC 600mA.How to design the transformer? I need the transformer parameter. Please help me.