Hi,
I have a problem to integrate a BQ2004 into my design. It is to charge a 10-cell NiMH battery with C/2 current. On start up it immediately jumps into trickle charge and the LED outputs (in mode 3) show that fast charge is complete. TM1 and TM2 are set to VCC and Float, respectively. I do not use the discharge facility. TCO and TS are left open, INH is tied to VCC.
Looking at VBAT and VSNS gives VCELL = 2.4V, which is below VMCV and above VEDV.
Is there anything a novice user can do wrong with this charge controller?
Best regards - Max