Hi,
I am confuse about the cross frequency of TPS53319EVM-136. The cross frequency is about 11.63kH when the switching frequency is 500kHz. Why the EVM has so fast response at such low cross frequency? And what determines its bandwidth?
In addition, I pull the FB pin to gnd to test OVP. The Vout is increased, then the circuit latches OFF the high-side MOSFET driver and latches ON the low-side MOSFET driver, the voltage of LL is low and Vout is decreased as shown in picture. However, why the switches work again after that as shown in picture?