Hi,
Customer is considering LM25145 and TPS40170.
Customer required specification is;
□Vin=24V □Vout=10~14V(12Vtyp) □Iout=7A(max) □Target Fsw=200~300kHz
Under these conditions, which device do you recommend?
When comparing A and B, the specifications are quite similar.
Therefore, customer is in trouble with device selection.
Best Regards,
Yusuke/Japan Disty