I'm testing LM5035:
1. feedback loop disabled
2. A precision current source is connected to the COMP terminal.
3. I change the current at the input and monitor the change in PWM on transistors
Observations: there are current values at which the PWM on the upper transistor is 70%, and on the lower transistor only 3%.
It was expected that the chip should change evenly the duty cycle on both channels, taking into account the delays.
My circuit is not typical for this chip. Load 24 V, 30 mA (2 channels).
Transformer 4: 6: 6.
This decision was made to reduce the number of turns of the transformer windings
Thanks!