Other Parts Discussed in Thread: LP55281, LP5569
I would like to also be able to drive one of the LEDs with an external signal. I'm thinking I can just use a high side switch and series R from the Vout pin to the LED anode I wish to drive. Seems from the data sheet the outputs can be overdriven up to the supply voltage + .3V, though Vout could potentially be high than that?
The outputs shows as DAC controlled current source between Vout out and the LED drive pin.
Sketch showing idea attached. Can anyone comment on if this is OK or not?
Thanks.