A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As just discussed on the phone, I do not recommend to do that. I would expect problems with output voltage regulation accuracy and depending on the difference of the output voltage to the set fixed output voltage there is some risk to run into problems with control loop stability.
I recommend to use the TPS62175, which is the adjustable version in this family.