Other Parts Discussed in Thread: BQ24210
Hi,
What is the internally set termination current for a ICHG < 250 mA?
I have a 350 mAh battery but with a fast charge restriction to 0.5C so ICHG is 175 mA. In the Jan 15 datasheet, Electrical Specification only gives a value for > 250 mA (8-12%). In para 8.4.5.7 a figure of 20% is given.
Thanks,
Pete,