This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC5926: Wrong OUT pins sequence

Part Number: TLC5926


Hi there,

I'm using the TLC5926 to drive a couple of 7 segments led display.

I use the OUT0 for segment (a) and continue with it up to the decimal point in OUT7 (pin 12). The second digit start in OUT8 with the segment (a) but the sequence is inverted. In this case the OUT8 is the decimal point and finish with the OUT15 with the segment (a).

I was testing the connections and the datasheet but nothing explain this issue.

I have PCB boards manufactured with the wrong sequence.

I did something wrong?

Thanks.