This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3152: FET failure

Part Number: LM3152
Other Parts Discussed in Thread: CSD17527Q5A

We are using an LM3152MH-3.3 part with two CSD17527Q5A FETs to generate 3.3V from a 24V input. We have recently had 2 of these circuits fail and have found that one or both of the FETs have failed shorted. When I use TINA simulation software with these input/output voltages I see that the recomend FET is a CSD18537 which is a  60V part rather than the 30V part that we used. Is the 30V part too low a voltage rating for this application and the cause of our failures? The input power is from a VXI back plane and the rated supply variation is 24V +1.2/-.72 volts. The 3.3 is powering an FPGA and the current draw is not known, most likley well under 1 amp.

  • John,

    I would recommend a FET with a higher voltage rating. The SW node can overshoot/ring many volts (VIN + many volts) depending on part selection and layout.

    Check the switch node with a scope to see what kind of overshoot you're getting. That's probably what's causing these failures.

    -Sam