Other Parts Discussed in Thread: TPS63710, LM27761, , TPS65131
Hi DC/DC team,
I am looking for a recommendation for a customer solution in with one of our parts. Essentially they will have +5V rail and need to create another rail from -5V to -10V. The maximum current output should be no more than 500mA. Size is a major concern.
My first look was at the TPS63700 and TPS63710. The LM27761 was also mentioned, but it has a limited output range and less current output capability.
Is there another part that could be interesting to promote?
Feel free to reach out to me over email if you would like to hear more about the opportunity as well.
Thanks!
Paul
DC-DAC Applications Team