Other Parts Discussed in Thread: LMZM23601
Hi,
I am designing a multiple output dc-dc converter. The following is the spec.
Vin: 20 V-36 V, Vo1: 15 V/ 1 A, Vo2: 5 V/1 A, Vo3: -15 V/ 0.3 A.
Do you have any power module realizing multiple outputs? If not, do you have any suggestion for the design?
Thanks!