Other Parts Discussed in Thread: TL431
Hi,
I am trying to design flyback dc-dc converter using LM3481. I have used the calculator software from Ti for LM3481 and simulated the circuit in ltspice for input 19V to 36V the output 24V.
This is working very good in ltspice and for confirmation I have also simulated 12V output circuit in ltspice with values obtained in calculator software.
Please see the circuit and simulation for 24V below
Can you please check this and let me know if there is a mistake?
Also, I am not sure that it is correct to attach 4.7K between Comp and VCC pins, I have just replicate it from LM3481 EVM?
Thank you.
Kind regards
Mohsin