This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF5025A-Q1: REF5025"A"-Q1 vs REF5025-Q1without A

Part Number: REF5025A-Q1

Hi

regarding REF5025"A"-Q1 vs REF5025-Q1without A 

REF5025-Q1 is listed in below, but when I click this part#, it jumps to REF5025"A"-Q1 Spec.

without A is invalid call out and correct part# is REF5025"A"-Q1?

www.ti.com/.../snva842.pdf

REF5025"A"-Q1

www.ti.com/.../sbos456h.pdf

  • Hi Taka,

    That is correct. We only offer REF5025A-Q1 which is 0.1% accuracy device. We do not offer the REF5025 0.05% accuracy device in Q100 grade. We are sampling the REF3425-Q1 which is similar performance to the REF5025 but this device is not released yet.

    -Marcoo