This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87524B-Q1: Where to tie the SCL and SDA lines when they are unused

Part Number: LP87524B-Q1


The datasheet for the PMIC does not mention what to do with the SCL and SDA lines if they are unused. Since the board will not have a 3.3V supply until after the PMIC is turned on, should they be tied to the 3.3V output of the PMIC or tied to ground?

Additionally, if they are tied to the 3.3V output should this be done through a pullup or straight to the rail?

Thanks,

Kevin