Hi
I would like to simulate TPS4H160A-Q1 device in TINA TI. I got the TINA reference design for the B model of the same part number but i am in need of Version A model for this device. Please help
Thanks and Regards
Manoj Shenoy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I would like to simulate TPS4H160A-Q1 device in TINA TI. I got the TINA reference design for the B model of the same part number but i am in need of Version A model for this device. Please help
Thanks and Regards
Manoj Shenoy
Hi,
Yes version A is having separate status for each channel. I would like to simulate my use case with version A model before finalizing.
I have one more doubt. The current limit feature through CL pin is for individual channel or as a whole IC? Let say if 2.5A. Is it for one channel or as a total?
Thanks and Regards
Manoj Shenoy
Hello,
I need to work with the simulation team for generation a model for A version but not sure how long it takes.
External resistor on current limit pin is for individual channel. And all channels have the same current limit within the specified tolerance. If you calculate the external resistor Rcl = Vcl x Kcl/Iout and Iout = 2.5A, so single channel current limit is 2.5A and not the whole IC current. The nominal whole IC current is 4 x 2.5A = 10A.
Regards
Hi Mahmoud,
I have one more query related to the maximum current
In the datasheet its mentioned the internal current limit maximum is 14A. Does this mean for each channel its 14A? If not what is the maximum current limit for each channel.
Thanks
Manoj Shenoy
Hello Manoj,
Yes, the specified internal current limit is per channel. Each channel has internal current limit of 14A max.
Regards
Hi Mahmoud,
Yes. It resolved my query. Thanks for the detailed reply.
Thanks and Regards
Manoj Shenoy