This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170-Q1: Max VIN 150V for generator/alternator use

Part Number: LM5170-Q1
Other Parts Discussed in Thread: LM5170

Hi,

I'm working on a PMU (Power Management Unit) for a three-phase generator that delivers up to 85VAC rms at no load. That should be over 100V after rectifying and filtering. The final DC/DC output should be 50V 100A Our idea was to use the new LM5170-Q1, however the absolute maximum rating on the HV-port is 100V. Any way to increase it using the "trick" described in this blog?

Looking forward for a suitable solution.

Thanks!

-Jarno