Hi, I would like to create a current source circuit with the following:
- Able to drive ~20mA ± <50µA and ~140mA ± < 2mA current
- Prefer 8 channel or more
I came across the TLC59213 and see the current spec and channel count fit my need perfectly.
But I am not sure if this chip can help provide a stable current for LED driver application.
1. I saw the Link alt_slvs867b.gif Can this design help provide stable current if I try to choose a high precision Y1-Y8 in the diagram?
2. If this current source solution doesn't meet my accuracy, do you have any other suggestion IC which can help achieve this?
3. Can this chip also do Continuous Pulsing Current? If not, any suggestion chip you have?
Thanks for the help.