This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65930 VBUS issue

Hello

In our application we do not need VBUs, we have pulled up Vbus pin to 5V through a 10k resistor. When we ran the system it complained from Vbus error. I changed the pull up resistor to 1k ohms then things went ok for one day only, afterwards we kept getting VBUs error. It looks like pulling vbus up to 1k Ohm did caused some damage, Do you think this possible to damage the part because of 1kohm? We did not disable the CP  and our ID pin is grounded. if we disable the C.P. do you think the Vbus detection logic will be disabled too?

Thanks

Feras