Part Number: BQ24296M
Other Parts Discussed in Thread: TPD1S514, BQ24296
Hi all,
I'm using the BQ24296M IC in a charging circuit design. I noticed that the resistance between the SYS output and GND started in the tens of kΩ and slowly decreased to ~0.8Ω currently as the board was powered (no battery connected, VBUS = 5V). The resistance is measured when the board is powered off. This occurred over ~1-2h of total powered-on time while I was testing other parts of the circuit. The low resistance triggered the overcurrent protection, SYS fell to 0V and the LEDs (STAT and PG) turned off. Before completely dying, the LEDs behaviour degraded (randomly flickering and being dim). Needless to say that the IC is destroyed.
Furthermore, I noticed that the resistance between SYS and BAT (essentially the resistance of the BATFET MOSFET) also decreased; to around 66Ω this time. I believe that this mostly happened while a cell was connected between BAT and GND, but I cannot say with certainty. In addition, I noticed that the SCL, SDA and CHARGER_INT pins were not pulled to 5V as they should from the pull-up resistors. This indicates that (at least some parts of) the internal circuitry was also shorted/destroyed in the process, which pulled these pins down to ~0-1V in my case.
I can say that no cell was connected for 90-95% of the time for which the board was powered (as I was testing other circuit sections, not related to the BQ24296M). Also, the IC never got hot and no external components were damaged. This behaviour happened with two chips. Below is the circuit schematic. The CHARGE signal is connected to the Lithium-ion cell's cathode through a relay. OTG is no-connect.
Does anyone notice a schematic error which could result in the chip slowly destroying itself?
Thank you very much,