This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92662-Q1: Unused pin connection check

Part Number: TPS92662-Q1

Hi, all. If we do not use ADC22,ADC21,AREF2,RX,TX,CLK pin, how to deal with these pins?

  • For ADC input, can we connect them to GND?
  • AREF2 connect with 10nF capacitor?
  • RX, TX,CLK all connect with one 10k resistor to ground?