Hello,
I am using the LM5170Q calculator.
I want to use 6 phases.
i choose the ripple I want to achieve. the result I get is that the more phases I add the larger each phase inductor I need.
when working with interliving multiphase the result shout be the opposite.
as much phases I have, each inductor should be smaller due to interliving ripple cancelation.
How can I calulate the inductance needed to get 3% ripple current with 6 multiphase interliving? (that is a buck current source)
Thank you,
Mor.