This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: Detect range and accuracy

Part Number: BQ76930


Hi, team:

My customers have some questions. Please help to answer them, thank you!

(1) The cell voltage detect range mentioned in the BQ76930 datasheet is 2-5V. When the cell voltage is below 2V, what will the IC report?

(2) What is the accuracy of the current acquisition accuracy of the BQ76930 in practical applications?

(3) One button switch connected to TS1 on the datasheet(the output is only available after REGOUT is pressed). The start time Tboot given in the datasheet requires a maximum of 2ms. It is impossible to connect one such switch in actual product. After power-on, press the button to switch the chip to have output. It can only be controlled by the MCU (this takes up an IO port of the MCU). Can the button switch be shorted without the button switch?